Hard disk drives are today's fastest permanent storage media and have a large capacity. For this two reasons they are the most used storage medium in computers and servers. When buying a new hard disk, there are three important things to consider: - The connection of the disk to the computer or other device you will be using it with has a big influence on the speed with which data can be read from/written to the disk. Make sure the connection of the disk you buy is compatible with your computer! - The rotational speed is also important for the speed with which data can be read from/written to the disk and determines the time it takes to find a file on the disk. - Last but not least, the storage capacity of the disk, i.e. the amount of data that can be stored on the disk.
Release date: 08 Sep 2007
Info modified on: 03 Jun 2009 10:30:11
Product views: 0
This statistic is based on the
6819
using ecommerce sites (eshops, distributors, comparison sites, ecommerce ASPs, purchase systems, etc) downloading this ICEcat data-sheet since
08 Sep 2007.
Only sponsoring brands are included in the free Open ICEcat content distribution as used by
6328
free Open ICEcat users .
Hard disk drives are today's fastest permanent storage media and have a large capacity. For this two reasons they are the most used storage medium in computers and servers. When buying a new hard disk, there are three important things to consider: - The connection of the disk to the computer or other device you will be using it with has a big influence on the speed with which data can be read from/written to the disk. Make sure the connection of the disk you buy is compatible with your computer! - The rotational speed is also important for the speed with which data can be read from/written to the disk and determines the time it takes to find a file on the disk. - Last but not least, the storage capacity of the disk, i.e. the amount of data that can be stored on the disk.
Specs
Alternatives
Options
Disk drive
Hard disk drive capacity
The maximum storage capacity of the hard disk in gigabyte (1 GB = 1 billion bytes).
160 GB
Internal
The device is built in, or needs to be built in (Yes/No). No, means that the device is connected externally via wire or wireless.
Hard disk rotational speed
The rotational speed of a hard disk expressed in rotations per minute. The faster the better.
7200 RPM
Hard disk interface
Serial ATA
Hard disk size
2.5 "
Connectivity
USB 2.0 connectors
1
Weight & dimensions
Weight
Weight of the product without packaging (nett weight). If possible, the nett weight is given including standard accessories and supplies. Please, note that sometimes the manufacturer is giving a too commercial interpretation of product weight, by leaving out the weight of accessories and/or supplies.